What is IO-Link?

THE COMMUNICATION STANDARD THAT BRINGS DATA, DIAGNOSTICS, AND INTELLIGENCE DIRECTLY TO THE FIELD

In the past, the sensor/actuator level was rather limited: on, off, that’s it. Communication typically ended at the fieldbus level. Sensors and actuators usually provided only simple information such as “object detected” or “valve open.”

IO-Link extends this communication all the way down to the sensor/actuator level. The globally standardized and vendor-neutral communication standard (IEC 61131-9) enables bidirectional data exchange between the fieldbus level and sensors or actuators.

IO-Link does not replace a fieldbus, but rather supplements it with an intelligent connection all the way to the field. This makes the sensor/actuator level smarter: In addition to pure process data, diagnostic, parameter, status, and maintenance information can also be transmitted. Devices can be configured centrally, their status can be queried at any time, and maintenance needs can be identified early on. And best of all: Wiring is done using simple, standard 3-wire sensor cables.

WHAT DOES AN IO-LINK SYSTEM CONSIST OF?

AN OVERVIEW OF MASTER, DEVICES, AND CONNECTION TECHNOLOGY

An IO-Link system essentially consists of an IO-Link master, several IO-Link devices, and the appropriate connection technology. Together, these components ensure that information from the field is not only transmitted but can also be used intelligently. Communication between the IO-Link master and the connected IO-Link devices takes place via IO-Link. This is a point-to-point connection: exactly one IO-Link device is connected to each IO-Link master port. To connect the IO-Link system to the higher-level controller, the IO-Link master uses the existing fieldbus or Industrial Ethernet.

The IO-Link master serves as the link between the fieldbus or Industrial Ethernet level and the connected IO-Link devices. It exchanges process data cyclically with each IO-Link device and makes this data available to the controller via the higher-level fieldbus system (e.g., PROFINET, EtherNet/IP, or EtherCAT). In addition, when necessary, it provides acyclic data from the devices—such as warnings or error messages—and forwards this data to the controller.

IO-Link devices are devices with an IO-Link interface that communicate with the controller via an IO-Link master. These include, for example, sensors and actuators that can exchange not only process data but also parameters and diagnostic information.

Even conventional sensors and actuators without their own IO-Link interface can be integrated: IO-Link I/O modules capture their digital or—depending on the model—analog signals, or output the corresponding control signals. Since IO-Link is a point-to-point connection between a master port and a device, IO-Link communication in this case takes place exclusively between the master and the I/O module. Between the module and the connected sensors and actuators, however, conventional digital or analog signals are transmitted—not IO-Link. Since IO-Link is standardized worldwide, IO-Link devices can communicate with IO-Link masters from different manufacturers. A device description file, known as the IODD (IO Device Description), is available for each device. It contains the information required for parameterization and the correct integration of the device.

IO-Link devices can be integrated into various control and fieldbus systems via compatible masters. This enables flexible component selection, simplifies integration, and supports long-term investment security.

Unshielded sensor cables are sufficient for communication between the IO-Link master and the device. For IO-Link Class A, 3-wire cables can be used. If devices require an additional power supply and therefore fall under IO-Link Class B, 5-wire cables are used. Regardless of the IO-Link class, wiring effort is reduced, installation time is saved, and potential sources of error are minimized.

WHAT ARE THE POSSIBLE APPLICATIONS FOR IO-LINK?

FOR GREATER FLEXIBILITY, TRANSPARENCY, AND EFFICIENCY IN AUTOMATION

IO-Link extends the traditional sensor and actuator level to include end-to-end communication, parameter, and diagnostic data. This makes it easier to integrate field devices, adapt them flexibly to requirements, and monitor them specifically.

Parameters for sensors, actuators, and other IO-Link devices can be configured and managed centrally via the controller or the engineering tool. Changes no longer need to be made directly on the device—this simplifies commissioning and speeds up format or product changes.

The parameters and configuration settings of the IO-Link devices can be saved in the controller via the IO-Link master and automatically transferred to the new device if a device is replaced. This eliminates the need for re-parameterization and ensures rapid recommissioning.

A configurable IO-Link device can support different functions or measurement ranges. Instead of having a separate device for each application, a single device can be configured for the specific application. This reduces the number of variants, inventory, and procurement costs.

In addition to process data, IO-Link devices also transmit status and diagnostic data. For example, they can report contamination, limit violations, temperature increases, or device-specific errors. This allows for the early detection of anomalies even before a device fails, enabling better planning of maintenance measures and faster localization of faults in the event of a malfunction.

With IO-Link sensors or IO-Link converters, analog measurement values can be digitized directly in the field and transmitted as IO-Link data. This eliminates the need for the time-consuming installation of shielded analog cables. Digital transmission is also less susceptible to interference, more cost-effective, and can be assembled directly in the field if necessary.

IO-Link I/O modules consolidate digital or—depending on the model—analog inputs and outputs in close proximity to the signal source. Signals from sensors and actuators are collected there and transmitted to the master via IO-Link. Using an IO-Link I/O module, up to 16 I/Os can be transmitted via a single three-wire standard sensor cable—occupying only one port on the fieldbus module (IO-Link master). This shortens cable runs, reduces wiring effort, and simplifies installations in cable glands or drag chains.

What are the benefits of IO-Link?

MORE TRANSPARENCY. LESS DOWNTIME.

No more silent sensors, hidden faults, or unnecessary variety. With IO-Link, field devices can be addressed individually, provide diagnostic information, and be configured directly from the controller. In this way, IO-Link creates transparency and lays an important foundation for Industry 4.0 and predictive maintenance.​

Simple Wiring with More Features

IO-Link significantly reduces wiring effort: Despite extensive parameterization options and additional functions, connection is made via a standard three-wire sensor cable. This simplifies installation and lowers connection costs.

Greater Transparency in Plant Operations

Additional equipment information provides a more detailed view of the system's condition. This makes it easier to classify anomalies and pinpoint the source of malfunctions—an important foundation for making informed operational and maintenance decisions.

Higher System Availability

Detecting changes early on can help prevent unplanned downtime. In the event of a malfunction, accurate diagnostics and streamlined replacement processes facilitate a quick return to operation.

Less effort required for commissioning and service

Device parameters can be configured and managed centrally. This saves time, reduces potential configuration errors, and simplifies recurring tasks—from initial startup to maintenance.

More flexibility with fewer variants

A smaller variety of parts simplifies procurement and spare parts management. At the same time, changes to the system can often be implemented using existing components—which saves effort and provides greater flexibility.

Lower costs over the life cycle

The economic benefits extend from installation through ongoing operation: Lower material and installation costs, a more streamlined spare parts inventory, and more efficient service processes can reduce a plant’s total costs.

MORE THAN JUST COMPONENTS. A COMPLETE IO-LINK SYSTEM.

THE RIGHT COMPONENTS FOR YOUR SMART AUTOMATION.

A comprehensive IO-Link system is created through the interaction of high-performance components and a suitable automation concept. This is exactly where Murrelektronik comes in: We view IO-Link not as a standalone interface, but as part of an intelligent, decentralized automation solution. ​With high-performance IO-Link components, modular concepts, and expert technology consulting, we create systems that work today and can scale with your needs tomorrow.​

A high-performance IO-Link system is created through the interaction of masters, IO-Link I/O modules, and other devices. Discover our solutions for seamless and reliable communication:

IO-Link simply makes machines more efficient, flexible, and cost-effective—Murrelektronik ensures future-proof data transmission.
Wolfgang Wiedemann, Director Application Sales Consulting, Murrelektronik

Applications of IO-Link

IO-Link is well established in many industries—anywhere sensors and actuators are used to control processes

Automotive Applications

Automotive production is characterized by numerous variants, short cycle times, and high quality requirements. IO-Link brings intelligence down to the sensor and actuator level: Additional process values, as well as diagnostic and event information, lay the foundation for high process transparency. This data can be collected, visualized, and analyzed to detect anomalies early and optimize processes in a targeted manner.

IO-Link devices can also be configured centrally via the controller and IO-Link master. A configurable device can thus cover different functions or settings and replace multiple device variants. This simplifies commissioning and reduces the effort required for model changes.

Intralogistics Applications

In conveyor and sorting systems, a continuous flow of materials is crucial. Especially along long conveyor routes, IO-Link enables a cost-effective, decentralized installation concept: IO-Link I/O modules bundle the signals from conventional sensors and actuators directly on-site and transmit them to the IO-Link master. The proximity to the signal source shortens cable runs, reduces wiring effort, and simplifies installation.

Where additional flexibility and intelligence are required, sensors and actuators with an IO-Link interface can be connected directly to the master. They enable centralized parameterization and provide not only switching states and measured values but also status and diagnostic data.

Packaging Application Area

Packaging systems often consist of several physically separate subsystems with different requirements. During product and format changes, IO-Link devices can be centrally configured and adapted to the respective product. This simplifies changeovers and ensures reproducible settings.

At the same time, IO-Link enables the efficient connection of these subsections via IO-Link masters and decentralized I/O modules. This allows components to be specifically selected for each section of the system. For example, only the components in the wet area need to meet the protection and cleaning requirements specified for that area. This optimizes component selection and enables a cost-effective installation concept tailored to the individual sections of the system.

Application Area: Machine Tools

Machine tools require precise processes, high availability, and rapid troubleshooting. IO-Link transmits process values as well as device, status, and diagnostic data from the sensor and actuator level to the control or OT level. This enables, for example, the early detection and analysis of limit violations, temperature increases, or device-specific errors.

Centralized parameterization simplifies the commissioning and configuration of devices. Depending on its range of functions, a single device can perform various tasks and replace multiple device variants. This simplifies variant management, procurement, and inventory management. Decentralized IO-Link I/O modules also bundle signals directly within the respective machine area, reducing the amount of wiring required throughout the machining process.

Renewable Energy Applications

Wind turbines, solar systems, and electrolysers require high availability, scalability, and easy maintenance. IO-Link enables cost-effective, decentralized installation—even under demanding environmental conditions and in hard-to-reach locations. Short cable runs reduce wiring effort, while modular designs simplify system setup and expansion.

Centralized parameterization and transparent diagnostic data simplify commissioning, facilitate fault localization, and support condition-based maintenance. In appropriately configured systems, stored parameters are automatically transferred to compatible replacement devices. This speeds up device replacement, reduces downtime, and supports reliable plant operation.

WE SPEAK YOUR LANGUAGE AND THAT OF YOUR PRODUCTION

IO-Link connects components, systems, and people through a standardized communication protocol. Together with you, we lay the foundation for future-proof production processes. ​

Contact us now!​

FAQ: Questions and Answers About IO-Link

Explained clearly and in an easy-to-understand way

Yes, IO-Link can be easily retrofitted into existing systems. Depending on the application, a complete IO-Link system—including IO-Link masters, sensors, actuators, and other components—can be integrated. Since IO-Link is based on a standard unshielded three-wire cable, existing cables can often be reused. This allows the system to be modernized and expanded with additional diagnostic and parameterization capabilities without the need for extensive rewiring.

No. Communication takes place via a standard unshielded three-pole cable.

In addition to process values, IO-Link also transmits diagnostic and status data. This allows for the early detection of issues such as contamination, limit value violations, communication errors, or an impending device failure. Maintenance measures can be planned more effectively, and faults can be pinpointed more quickly.

If the device parameters are stored in the IO-Link master, a compatible replacement device can automatically be configured with the saved settings when it is installed. This reduces the need for manual parameterization and speeds up the recommissioning process.

IO-Link provides the foundation for making data from the field level available in a structured format. Sensors and actuators not only provide measured values, but also parameter, diagnostic, and status information. Via IO-Link masters, this data can be transmitted to controllers, edge systems, or higher-level IT and IIoT platforms and used to enhance transparency, enable analysis, and optimize processes.

IO-Link is particularly well-suited for applications in which a large number of field devices need to be integrated, flexibly configured, or reliably monitored:

  • Machines and systems with many sensors and actuators: IO-Link I/O modules consolidate numerous inputs and outputs directly near the machine. The collected signals are transmitted to the master via a single IO-Link connection, where they occupy only one port. This reduces cable runs, wiring effort, and the need for additional fieldbus components.
  • Greater intelligence at the sensor and actuator level: Additional process and diagnostic data make it possible to provide transparency into system status, detect anomalies early, and
  • optimize maintenance and processes.
  • Simpler and more cost-effective wiring: Standardized, unshielded three-wire sensor cables reduce the need for special cables and adapters. Decentralized IO-Link I/O modules bundle signals directly at the machine and transmit them to the master via a single connection. This saves on cable runs and installation effort.
  • Centralized parameterization for flexible use: IO-Link devices can be parameterized centrally and—depending on their range of functions—adapted to different tasks. This reduces the number of device variants required and simplifies procurement and inventory management.